Part Number: SN74LV6T17 Other Parts Discussed in Thread: TXV0106 Hello team,
Can I input 1.8V to the input pins, when the device is powered OFF?
I see, there is no clamp diode from input to Vcc, so I am assuming its okay.
Best Regards, Kei Kuwahara
Hi All,
Please see the new TXV level-shifter family (TXV0106-Q1 / TXV0108-Q1) supporting high-bandwidth timing-margin sensitive interfaces such as RGMII.
For more information, see Enabling high performance interface translation | Video | TI.com , thanks…
Part Number: SN74AXC4T245 Other Parts Discussed in Thread: TXV0108-Q1 , TXV0106-Q1 Hi Team,
We are using the SN74AXC4T245PWR IC for level translation. In the datasheet, it is given that the data rate supported whea.n translating from 1.8V to 3.3V is up…
Hi Jeff,
We actually released a new translator family specific to tight timing budget applications such as RGMII.
Please help see TXV0106-Q1 and TXV0108-Q1, thanks.
Best Regards,
Michael.
FAQ: Logic and Voltage Translation > Auto-Bidirectional Level-Shifters > Fixed DIR / DIR CNTRL Level-Shifters >> Current FAQ
Choosing a high drive strength device depends on the below:
Static DC drive strength: Drive required for a constant…
FAQ: Logic and Voltage Translation > Auto-Bidirectional Level-Shifters > Fixed DIR / DIR CNTRL Level-Shifters >> Current FAQ
When in doubt, use a 0 ohm series resistor on the outputs and adjust accordingly, for your system needs.
This can also…