Part Number: UCC27517A-Q1 Hi Dear
I have been informed of the following question from customer.
Has UCC27517A-Q1 already been qualified for AEC-Q006 ?
If not yet, would you please tell me when it will be?
Part Number: UCC27517A Other Parts Discussed in Thread: UCC27517 I am using a UCC27517 as an alternate to SN74LVC3G Buffer. As per the below waveform, the switching is at 5MHz and the current is almost 60mA.
The UCC27517 is used as a low side to turn on…
In hybrid electric vehicles/electric vehicles (HEV/EV), the engine is not used to run the heating and cooling system like it is done in the internal combustion engine (ICE) vehicles. To replace this function, two key systems are being used: a BLDC motor…
Part Number: UCC27517 My customer uses UCC27517DBVR in production. Due to increased demand and long lead time he considers UCC27517 A DBVR as a drop in replacement.
Is this possible?
Thanks Josef
Hi Arghya,
Thanks for reaching out to TI.
We currently do not have a SIMPLIS model currently for this device. Is there a limitation to using the PSPICE model?
Additionally, I do also want to mention that we do have an "A" variant in the UCC27517A that…
Part Number: UCC27537 Other Parts Discussed in Thread: UCC27517A , LMG1210 Hello
Some MOSFET has drive source and power source. How do I connect the driver with the MOSFET.
Like Infineon IPDQ60R010S7, the part has power source and drive source.
Normally…
As shown in section 6.3, the highest AHCT supply voltage would be 5.5 V.
To convert to a voltage higher than nominally 5 V, you need a CD4000 device like the CD40109B-Q1, or a gate driver like the UCC27517A-Q1.
Part Number: UCC27517A Other Parts Discussed in Thread: UCC23511 , UCC23513
Hi, everyone. I use gate driver have some questions need to help. Below design often used to driving BLDC. The bootstrap Cap and diode are used to supplying the voltage to High-side…