Ok, figured out few things related to my previous post:
*1) The OPA2889 can operate on a single supply voltage as low as 1.8 - 2.0v. This is great for MSP430 applications with voltages as low as 1.8v. The gain will be reduced ofcourse, but its still…
Part Number: LM3481 We are referring LM3481 application note for designing Non-Isolated Fly-back converter. For that we are going through the design formulas given in application note.
In the application note of LM3481, there is one equation to calculate…
Other Parts Discussed in Thread: DRV8302 Hi,
I am trying to use the DRV8302 to drive a BLDC motor. When I set EN_GATE to high, the FAULT pin goes low and all gate outputs are zero. I went through all the possible conditions in the datasheet, but none…
lm2907-n.pdf
I am just a little confused reading a data sheet on the LM2907. The datasheet I am reading the datasheet SNAS55C-June 2000-Revised March 2013. The equation for Vout on page 1 is given as, Vout=fin*Vcc*R1*C1. But on page 8, the equation…
Hi steven,
thanks for your input.
1. What input voltage will be used? Is OVP not required (input FET is not blocking input adapter OVP)? What is the current limit for the input?
-> The input is connected to the adapter (5.0V/4A) through the eFUSE…
Hi Leo.
I asked how to flash an MSP430F2112 by serial interface using its emebedded BSL.
Following your kind suggestion, I was able to find the BSLDEMO2.exe serial flasher inside the slau319c.zip package.
This flasher is classified "deprecated"…
Hi Archit,
Attached the pre-built boot partition which successfully boots to Linux (its a tar.gz file). Please let us know if this works (you may want to run env default -fa and saveenv on the first boot).
Regards
Shravan
boot.tar.gz.txt
Part Number: TMS320C6455 Tool/software: TI-RTOS Hi
My tools: OS: win7 Board: Customized CCS: V7
I want to make a DSP/BIOS project and add NDK to it, so I made a project as below:
I added NDK library as below:
when I build the project some…
Hi Srikanth,
Q1. What is the reason for this behavior. Specifically, what made the image boot successfully when placement was changed to MSMC or DDR3?
[Ivan] - By default, NOR boot does go through IBL and uses the first 0x20000 bytes. If you have…
Hi,
Below are my comments.
Q1: Is this a recommended pairing?
Rep: Ideally not. But depends on your application.
For example,
a) is the application intended only to read data from BLE devices and then send it to the remote cloud over Wi-Fi…