Part Number: UCD9081 Tool/software: Hello everyone,
I am trying to communicate with a UCD9081 device through the FT4232H of an FDTI chip.
Has anyone tried this and knows if it works or it can work only with the USB Interface Adapter Evaluation Module…
Part Number: UCD9081 Other Parts Discussed in Thread: USB2ANY Tool/software: Hi,
We utilize UCD9081 on our new design.
For programming UCD9081 via I2C;
1-We use USB2ANY (HPA665) to debug/confıgure interface of UCD9081.
2-We can read and probe I2C data…
Part Number: UCD9081EVM Other Parts Discussed in Thread: UCD9081 Tool/software: Hi,
I try to read the UCD9081 Device ID of 0x55 from register 0x27, but it reports 0x00. I use a custom USBC to I2C bridge board for this purpose.
Br,
Mozhdeh
Part Number: LMZM33602 Other Parts Discussed in Thread: UCD9081 Hello All,
We are using LMZM33602 Power Module in our design. Please review SYNC Connectivity of the attached Schematic snippet.
LMZM33602 will be in disabled state by default because of the…
Part Number: UCD9081 Other Parts Discussed in Thread: USB-TO-GPIO2 , I believe I have parts that were corrupted during programming because of greater that 32 byte block size and/or not programming complete device. These parts had prviously been reconized…
Part Number: UCD9081 Hello expert,
Does UCD9081 has .hex file could provide to 3rd party programming? My customer would like to program UCd9081 but their 3rd Party would like to have .hex file to program UCD9081. Thanks!
Best regards,
Ann Lien
Part Number: UCD9081 Other Parts Discussed in Thread: UCD9090 Hi experts
I have a question on UCD9081 and UCD9090.
What is the maximum Flash write duration expected for the part? Is it possible to put an upper bound on the time it takes to write the flash…
Part Number: UCD9081 After I powered on my board and configured the chip, after I clicked shutdown, there was a continuous level of about 1.9V on MON5 and MON6. After I disconnected the power supply I connected to, this level also existed, so it should…
Part Number:
1.udc90xxx_fireware_dmp.pl ucd90xxx_dataflash_dpm.pl Does ucd9081 support programming using these two pl files?
2.Minerva 3 PWR Sequencer Mar16 2023.par U63_UCD_SEQUENCER_MINERVA_3.hex How to convert ".par" and ".hex"…