Part Number: WILINK8-WIFI-NLCP Other Parts Discussed in Thread: WL1801 , WL1835 Hi,
1. Does Wilink8 mesh package support Non-TI platform with linux OS?
If so. Any limitation??
2. Does Wilink8 mesh work well with ALL wilink8 model? Can mesh work with single…
Hi.
WiLink8 may be connected to MCU via SPI interface. TI doesn't directly support this effort. 3rd party Clarinox may be able to assist you with this. Their contact info can be found @ https://www.ti.com/tool/WILINK8-WIFI-MCP8
Thanks
Part Number: WILINK8-WIFI-MCP8 Hello,
I tried contacting the listed contact person from Mentor( Andrew Caples ) without success. Here is the error that I got back(esa1.mentor.iphmx.com rejected your message to the following email addresses:).
Do you have…
Part Number: WL1837MOD I've been asked to create solutions for certifying a wilink8 enabled device. The goals requested are: for wifi: transmit at max power for all cannels and frequencies via wifi receive at every channel and frequency via wifi configue…
Part Number: WL1837MOD Hi Team WiLink,
I see from ( http://www.ti.com/tool/WILINK8-WIFI-MCP8 ) “The MCP package contains the install package, pre-compiled object and source of the proprietary Wi-Fi Driver - QNX, Nucleus, WinCE as well as ThreadX …
Part Number: WILINK8-WIFI-MCP8 Hi,
Trying to checkout oreo release. But gets below error
repo init -u git://git.omapzoom.org/platform/omapmanifest.git -b 6AO.x -m RLS_6AO.1.0.xml fatal: unable to connect to git.omapzoom.org: git.omapzoom.org: No address…
Part Number: WILINK8-WIFI-MCP8 Other Parts Discussed in Thread: CC3120MOD Tool/software: Linux Hello,
We are using iMX6 solo platform with linux, wanted to interface wi-fi module for the same.
1. Is it possible to interface simple link module CC3120MOD…
Hi Luke,
I am sorry, I am not able to comment whether TI have any roadmap to solve this issue, because I am not TI employee.
But if you want to my own opinion, I would be sceptical. It seems that TI moved focus to new CC33xx devices instead older CC32xx…
Part Number: WL1835MOD Team,
-Will the WL183x R8.8 SW support included by default in the next Sitara Linux Processor SDK? or do you always need to manually add it using the instruction provided in the UG SWRU561A?
-The BT stack has been certified against…
Part Number: WILINK8-WIFI-MCP8 Other Parts Discussed in Thread: AM4379 Hi,
I want to use the 5g wifi function on AM4379, and furtherly, I will use the same function on s32v234.
I found that wilink8 chip may fulfil my goal, but there remains several questions…