Part Number: XIO2001 Hi,
My customer has one question. He is making PCIe daughter card connected with PC.
According to the PCIe specification, /PERST is high after minimum 100ms from 3.3V power-up of PC's mother board. However, his daughter card with…
Part Number: XIO2001 Hi,
My customer observed the following waveform of PAD01 pin on XIO2001 EVM. You can see the noise of High side.
This noise is same as CLKOUT6 which XIO2001 outputs. (CLKOUT6 is connected CLK pin).
*1. Does TI have any production…
Part Number: XIO2001 Are there any trace length restrictions for PCIe (Pin 87/88), (Pin 93/94), (Pin 80/81) of XIO2001PNP? The same pair length complies with the IC specification?
Is there a need for snake routing to increase the anti-interference ability…
Part Number: XIO2001 Hello team,
The datasheet shows the Power consumption data, but is this connected to a 1 PCI device? If it connects 3 same PCI devices, will the power consumption roughly triple?
Regards,
Sato
Part Number: XIO2001 Hi,
Could you please support XIO2001 device as follows? In other words, does XIO2001 support “PCI<->PCIe” function on PCI bus card? Please advise us.
Thanks and best regards, M.HATTORI.
Part Number: XIO2001
Hello, my design is to expand two PCI slots with xio2001,There are the following PCB layout questions:
1、Should the routing length of the clock signal pciclk1 connected to PCI slot 1 by xio2001 be equal…
Part Number: XIO2001 Hello!
Please tell me that the configuration EEPROM model EVM of xio2001zgu is recommended to use 24LC08. Can 24C02 be used instead?
thank you!