Part Number: XIO2001EVM Other Parts Discussed in Thread: XIO2001 We are using an XIO2001EVM board on an NXP T1042RDB evaluation board (under a yocto linux) to check compatibility before to design our own hardware.
On XIO2001EVM board, we insert a PCI…
Part Number: XIO2001 Hi,
I'm interested in using the XIO2001 component i n safety critical avionics , and in order to certify the project we need to assess the design aspects of the COTS devices used in the card (including TI’s devices). Related to…
Part Number: XIO2001 Dear Sirs,
Is there a way to know if internal reset is active in XIO2001? Can I read GRST# pin to know if internal reset is happening?
Thank you
Part Number: XIO2001 Dear Sirs
We are debugging one card with one XIO2001 and one PCI softcore in Xilinx FPGA. The PCI softcore is used in many other designs and its behavior is well known. Sometimes after system up we see PRST# pulses that reset PCI…
Part Number: XIO2001 Hello,
we have components here with the following date code: $4A-43C2R2W.
What does this mean in detail?
Is there a decoding for the XIO2001 or where can I find a decoding?
Best regards
Nils Panitzsch
Part Number: XIO2001 Hi Team,
we got two pictures of different marking of XIO2001IZWS. please assist to check and advise the differences. thanks.
Regards,
Renee
Part Number: XIO2001 Hi,
Please tell me the following specifications of XIO2001 corresponding to PEX8112.
<<Recommended Operating Conditions>> ・VN - Negative Trigger Voltage [V] (3.3V buffer) (Min, Max) ・VN - Negative Trigger Voltage [V] …
Part Number: XIO2001 Hello. According to the XIO2001 datasheet, the Vrx-DIFF-p-p MAX voltage is 1.2 V. Is there any risk if the voltage is over than 1.2 V? The Vrx-DIFF-p-p MAX voltage of a board made by our company is about 1.5 V.
The COMMENTS says 「VRX…
Part Number: XIO2001 Hello,
I am investigating the maximum surface temperature of the IC with respect to the solder bonding ratio of the Power PAD. I know that a solder joint ratio of 50% or more is recommended, but I would like to know the maximum surface…