Part Number: XIO2213B I can't read back PCIE register value of XIO2213B in Linux (it always 0xff) , but i can read these register data in Windows . Do I need any Linux driver? My Linux is Ubuntu 22.04
Part Number: XIO2213B Other Parts Discussed in Thread: XIO2001 Hi,
We use the XIO2213B in our prodect, and now, we want to know if there are any program to suppor the extend EEPROM connect to XIO2213B, thanks.
Part Number: XIO2213B Hi, support team
My customer has the questions as follow:
Is there any way to identify which version A or B of XIO2213 is inside an Expresscard34(Sonnettech) without taking it apart? Device Manager lists the Device ID as 823F, but…
Part Number: XIO2213B Hi Team,
The customer's PCI-E Connect to 1394 DAQ then the system will be crashed. Do you have the last version of firmware for XIO2213? thx
Part Number: XIO2213B Hello,
About the XIO2213, I have some questions to confirm:
1. About the REFCLK+/REFCLK-, if it could accept 100MHz LVDS input clock. As the datasheet described, what is the common voltage of REFCLK?
2.CPB input threshold voltage…
Part Number: XIO2213B
PCIe Differential Reference Clock Input
1Vid range:0.0675V~0.6V , is it right ?
2What is the Vicm range? Is the LVDS level OK?
3The XIO2213B design has no internal 50-Ω-to-ground termination resistors. Both REFCLK inputs, at approximately…
Part Number: XIO2213B
What compliance or verification testing can be done once theXIO2213B is laid out on the board to ensure compatibility with other systems? Does the 1394B standard have tests that can be published to demonstrate interoperability with…