Part Number: TLV9001-Q1 Hi Expert,
Have a nice day! I have question about TLV9001-Q1need your professional support:
For Fig. 7-11:
1. Is the “ Gain ” in green circle Vo/Vi, and is the “Gain(dB)” in red circle 20log(Vo/Vi)?
2. What does “Gain…
Part Number: TMUX1308-Q1 Hi team,
I would like to confirm the output(D) status of TMUX1308-Q1 when EN=High. In this case, output D will be Hi-Z and voltage could be unstable? If we need a firm Low output in this case, a pull down resistor at D is required…
Part Number: LM74700-Q1 Hi expert,
From the datasheet in LM74700-Q1, it mentioned that there is a regulated conduction mode to regulate the drop out voltage to 20mV with a close loop. Then what if that customers select a MOS with small Rdson and the…
Part Number: BQ25692-Q1 Hi expert,
My customers are searching a charger for charging 5s supercap and they found BQ25692-Q1. They have following questions:
For this device in standalone mode, the Vreg, ICHG is set for the Li-ion battery, correct? Can…
Part Number: LM74700-Q1 Hi team,
Could you please share your comments for below questions?
In Reverse Current Protection Mode, is it possible to achieve zero reverse current? And the MAX reverse current is -11mV/Rdson.
However, in the Regulated…
Part Number: DRV8143-Q1 hi
I am using DRV8143 SPI(S) Variant in my circuit.
There are some problem to control the chip with ESP32-S3 via SPI.
I can read Devie ID of the DRV8143 and device ID is 0xBA.
And these are all register values of the chip…
Part Number: TPS62A01A Hi Teams,
The customer uses TPS62A01ADRLR with UWB chip in the rear stage. The above picture shows that a PMOS tube is used as a switch, and when the PMOS is turned on, the 3.3V power supply drops.
UWB has 3 10uf capacitors…
Part Number: TPS92692-Q1 Hi Team,
We are using the TPS92692-Q1 in boost mode in our design. The input voltage ranges from 9–36 V, and the LED driver is controlled using a PWM signal (1 Hz to 67 Hz) with a 1 ms ON time. The output is approximately 48…
Part Number: AM62A7 I am inquiring about the current ti platform's recommended methods for training model and deploying them on am62a soc. currently, I am using the edgeai benchmark tool, but I am encountering an error:" node kernel init failed"
Part Number: TXH0137D-Q1 Dear Experts,
I would like to know if the final mass-produced model of TXH0137D-Q1 will be packaged in TSSOP16 or TSSOP14. The data manual shows it as TSSOP16, but the order information shows it as TSSOP14. Please help confirm…