Part Number: TDC7200EVM Other Parts Discussed in Thread: TDC1000 Tool/software: WEBENCH® Design Tools I'know the board i'm mentioning is obsolete but this is important to my project. I have been trying to connect this board and have tried all the method…
Part Number: TIDA-00281 Other Parts Discussed in Thread: UCC27201A , CSD19535 I have two doubts about which I want very detailed explanations.
(1)According to TIDA-00281 its 1KW BLDC motor application with Vdc=48V. With this parameter, we can approximately…
Part Number: TMDSCSK388 Tool/software: Linux The customer has bought a new board csk388. He boot up by sd card. But he cann't see any image after he logged in the web ui. This is the log file.
U-Boot SPL 2016.05-00004-g63acf8c-dirty (Feb 13 2017 - 17…
Other Parts Discussed in Thread: TMDSHVMTRINSPIN , MOTORWARE , TMDSCNCD28035 , CONTROLSUITE Hello,
Is there any trouble i f I only want to DEBUG some program in CCS V6 without connecting the PC to TMDSHVMTRINSPIN?
If that is possible, which configuration…
Hi~
Out customer will apply TI RS485 device in RET(Remote Electrical Tilting).
As you know, RET system have many daisy chain.(max 32EA)
If see TI datasheet, it mentioned Unit Load(1/2, 1/4, 1/8) and Up to Nodes per Bus information.
In Case of…
Anshuman,
Now I use the version is 01.08.00.15, but there is a error when i run the demo, can you tell me how to set the parameter in the application?
setenv bootargs 'mem=128M console=ttyO2,115200n8 root=/dev/nfs rw nfsroot=192.168.47.197:/work…
HI Arun,
I build the application is use "make -s sys_all" and "make -s dvrapp" ,then "make fsupdate" . Whether i shoud use other commond to rebuild the M3 binaries, and how to rebuild?
when i set the bootargs is "setenv bootargs 'mem=128M console…
tda3 family.pdf dm505.pdf Sir,
Package information is not quite what I am looking for. I understand the package is FCBGA. What i want to know is the mechanical dimensions ( eg, width, height etc ) of the SOC. I will attach two files here- TDA3 datasheet…
Hi William,
When we use only resistive charges without the powerline (connected directly to the BOOSTXL) the sinewave stays clean even down to 2 ohms load.
This means that the AFE031's power amplifier is working properly.
When connected to the powerline…
HI TI,
I share the detail, when linux hang, trace32 cannot attach it, mcu1_0 CAN and serial is normal.
And after I remove ti_k3_r5_remoteproc ko and cdns3 ko, issue gone, Is there something debug I can do?
I attach Acore serial log,
TICE…