Tool/software:
Hello, I am looking to gather any details for the LM7321 op amp's die chemistry. Can you confirm this contains silicon? We are evaluating whether this is suitable for space or not recommended. On that note, any drop…
Tool/software:
Hello, I am looking to gather any details for the LM7321 op amp's die chemistry. Can you confirm this contains silicon? We are evaluating whether this is suitable for space or not recommended. On that note, any drop…
Hi Alex,
1. So, if you suggest still to add a series 3.32K resistor - your recommendation is also just to remove R5 (both GND's of both boards are connected) and to work as below:
Or the best will be to assembly also TVS instead of…
Hi Team,
My customer asks LM7321MF/NOPB Ibis model, however I can not find it on ti.com.
There are PSpice and Tina models on ti.com.
Can you share the lm7321 IBIS model if you have it?
Thanks and happy new year!
Taemin,
Dear, support team.
Our customer has a question on θjc in a 5pin SOP-23 package.
It has different θja in the model number even in the same DBV0005A Package.
LM7321MF/NOPB θja 325℃/W
OPA189IDBVR θja 134.5℃/W
LMP7701MF…
Hi Team,
Please help to provide the detailed RθJA test condition of LM7321 SOT-23 package (Air: still or moving, PCB:1s or 2s2p).
B.R.
Eric Ba