Tool/software:
I have my design back and it appears to be working ok but I have one issue. If I touch the input resistors, R901,R905, R907 in the layout, I can get the output to switch off. If I use a pencil or something else nothing…
Tool/software:
I have my design back and it appears to be working ok but I have one issue. If I touch the input resistors, R901,R905, R907 in the layout, I can get the output to switch off. If I use a pencil or something else nothing…
Tool/software:
Hi All.
on the data sheet of the TPS25947, there is the optional Oring connectivity pages 44-46.
TI writes - when the VIN1/2 are matched "current is shared between the rails in the ratio of differential voltage…
Tool/software:
Hi All.
i would like to connect two TPS259474ARPW in parallel in order to reduce the overall series resistor Rds on each item (two resistors in parallel) , the two items will get the same p[ower supply and will drive…
Tool/software:
Hi All.
i would like to connect two TPS259474ARPW in parallel in order to reduce the overall series resistor Rds on each item (two resistors in parallel) , the two items will get the same power supply in and will drive…
How can I use the OR gate in the grey zone? The eFuse is supposed to be enabled for 3V3, then the defined logics should come. However what I realized is that before even eFuse turns off, OR gate disables the device. So I pun a delay, it seems solved for…
Tool/software:
Hi All.
i have a question regarding, the TPS259474/TPS259480.
regarding the reverse current protection is see that in both items the reverse voltages : VREVTH can get very low down to 22.3mV/14.8mV in order to activate…
Hi Kazuya-san,
I apologies for delayed response.
Is it less than 21V because VIN absolute maximum is "VOUT-21V" (-40C~+125C)"
Yes, maximum 21V continuous voltage can be used.
Best regards,
Arush
Tool/software:
Hi Team,
Is it possible to leave FLT and AUXOFF of TPS259470ARPW open to reduce current consumption?