Dear Maximus Rusl The test pattern mode is a 60Hz pattern, the white point depends on the look selected a typical look will contain "Cool" look will have a duty cycle similar to ~50% green, 24% Blue, 26% red, you may get a similar white point running…
Sorry, but you didn't understand me properly I want to use MSP-FET. My question is can I burn with it both when the switch is in JTAG mode and in EXTERNAL mode? And what is the difference between the two burning options?
Second question, why do you…
Hi Kexiang,
If you have internal patgen with internal timing working then when you switch to external timing mode then you lose lock, there is one of 2 things happening.
Your external timing or clock is not working as expected from SoC (Video source…
Part Number: TMS320F28379D Tool/software: Hello Community,
I am having issues with my brand new TI Delfino F28379D Launchpad. I am trying to do a PIL simulation for my control algorithm in Simulink using this embedded controller for real-time closed…
Part Number: LAUNCHXL-F28379D Hello,
I'm using the TI Delfino F28379D LaunchPad with Simulink to receive an acquisition of sinusoidal current signals of three phase induction motor throughout a control drive. the timer period of epwm is 10kHz based…
Salah,
Looks like you are running the model in external mode at 100kHz. The ideal frequency for running in external mode 20kHz. As the external mode task is running in background, running at such high frequencies may not allow sufficient time for external…
Part Number: TMDSCNCD28335 Other Parts Discussed in Thread: TMS320F28335 , TMDSDOCK28335 Tool/software: Hello,
I have a TMDSDOCK28335 (TMS320F28335 Experimenter Kit) and I've been experiencing some problems when I use it with Simulink in external…
Hello Meet,
Meet Thakar said: Could you elaborate the issue further?
Sure. So I am trying to flash mcan_loopback_interrupt_am62px-sk_mcu-r5fss0-0_freertos_ti-arm-clang example application in external mode in ospi boot mode. And I have changed the…
KR BEE said: Hi, according to the datasheet. It is possible to configure the Vref to non-inverting input.
I am using LP-MSPM0L1306 launch pad and I tried to configure the OPA non-inverting input in system config but it shows '' the selected device is…