summary.bq.log.xlsx
Diego, I was able to capture data with Studio when a battery was in the confused state. Attached files for battery 1 (with bad SoC) and battery 2 (normal) at 5 times. Note that these 2 batteries are in one unit and going through…
Hi Badri, Thanks for the response. I checked both the places and its pal. But the irony is that for my display NTSC is fine. So when running this PAL settings I have changed the display standard through mcfw api (for that logs have attached). How to proceed…
Hi Badri,
Kindly refer to attached file, with file name ending '1' being the oldest, '3' the latest.
Fullscreen
4213.Vsys_printDetailedStatistics1.txt
Download
[m3vpss ]
[m3vpss ] *** Capture Driver Advanced Statistics ***
[m3vpss…
Dear Onyx san,
additional information. The SOC became 100% when SOCHold99 was changed from 1 to 0 (see below data).
190617_Charge.xlsx However, the charge current (111 mA) is higher than the taper current (66 mA) when SOC = 99 ⇒ 100%, and FC is never…
Other Parts Discussed in Thread: 4213 The attached presentation details how to make many common op amp circuits stable.
4213.Solving Op Amp Stability 2015_TG.pptx
Tamas,
yes that's REV0.
The ROM symbols changed between REV0 and REVA. Attached is the REV0 M-BootROM symbols library, the symbols are at
0x01006539 SelectEnet
0x01001bc1 EnetConfig
0x01000bf9 Update
0x20004534 mbrom_bmode
Try with these…
Matteo,
i am attaching CCS.3. project for an EMAC external loopbavk test. It also include the set PHY via MDIO. You import the project to CCSV5 and see what is needed for a basic transmission and reception.
4213.EMAC_LOOPBACK_EXTERNAL.zip
Thanks…
Hi Albert
Thank you for your help.
Have been resolved by changing the 8x link modify these examples of LLD.
Fullscreen
4213.Aif2_Cpri_LTE20MHz_8xlink_Test.c
Download
/**************************************************************…
Other Parts Discussed in Thread: OMAP-L138 , 4213 This problem was posted here also:
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/290173/1027881.aspx#1027881
I have a custom board which has the Logic PD Omap L138 SOM on it …
Other Parts Discussed in Thread: TMS320C6671 , 4213 Hello,
There are three keystone DSPs and one emulator port on my board.
EMU[0:18] signals are connected in parallel and JTAG signals are connected as daisy-chain.
Each DSP has its own boot loader…