Part Number: BQ78350-R1 Other Parts Discussed in Thread: 4213 , BQSTUDIO
Tool/software:
Hello,
We need help resolving why only cell 1 is getting discharged much faster than the other batteries in the battery pack (13S 2P) when the pack is left in…
Part Number: TDA4VM Other Parts Discussed in Thread: 4213 Hi, experts.
We're doing caculated performance test of DSP C66X, and compare the result with other manufacturers DSP(t he frequency of which is lower than C66X ). The result is worse.There is…
Part Number: SK-AM62 Other Parts Discussed in Thread: 4213 We want to use the jack audio input on the SK-AM62 (audio playback is working). The board runs the latest stock firmware 08.06.00.42.
Mic input is recorded with
arecord -f dat -t wav -D default…
Part Number: TDA4VM Other Parts Discussed in Thread: 4213 Tool/software: I am trying the SDK 9.2.
I run the default demo, it is running like this:
root@tda4vm-sk:/opt/edgeai-gst-apps/apps_python# python3 app_edgeai.py ../configs/object_detection.yaml…
Other Parts Discussed in Thread: TMS320F28379D , 4213 Dear team,
The device is TMS320F28379D. The doubts encountered when calling the sine and cosine functions in math.h:
#define sin __relaxed_sin
__inline double __relaxed_sin(double x)
{
return __sin…
Hi Timothy-san,
I resolved the issue for Win10 bellow.
Uninstall the driver
Install the driver with 4213.Driver_ProgrammingEVM_Windows7.zip (e2e.ti.com/.../317745)
Thank you for your support.
Best Regards,
Hiroshi Katsunaga
Part Number: UCD9248 Tool/software: Hi
I made a board with the same power supply configuration as VC707.(Using UCD9248)
Wrote the same software as VC707, and passed all.
But, no output from UD9248 When viewed in the Fusion Digital Power D esigned…