Hi Vinicius,
Sorry after a few week I have lost the context and now I don't have a full clear picture the issue any more, I need to review this thread again...
Vinicius Duarte said: In the new test I connect the pendrive to USB0 which is recognized…
Hello Yutaka-san,
Thank you for the note.
Yutaka Fukasawa said: We are going on a long holiday so I won't be able to follow you. very sorry. ( 4/26~5/6)
Noted.
Yutaka Fukasawa said: Could you please give me a final answer by May 7th?
Let me follow-up…
Part Number: AM3354 hello
The kernel I used was linux-3.2.0-psp04.06.00.11-04. When I opened CONFIG_USB_TI_CPPI41_DMA in deconfig, 335x used iperf as the server speed was normal, while the client speed was extremely slow. When I turn off DMA and use CONFIG_MUSB_PIO_ONLY…
Part Number: AM3354
Doing stress test on tens pcs of boards, there is a board, after launch up and leave there. after sometimes, some command is not available.
Any advice to identify this kind of issue.
yan ma said: Only a fraction of our machines have this problem, maybe two or three out of 20.
Have we booted the non-working boards ever?
The issue seems more correlated with HW board.
Best, -Hong
Part Number: AM3354 Hi,
Please kinldy review below pircture that we have got the sample MAC address from two AM3354 device, I know there are unique ID on every one device, thanks.
Level
Description
Part Number
Texture
BOM Customer Refe…
Part Number: AM3354 Hi Team,
Customer is asking for RoHS documentation for the following P/Ns:
AM3354BZCZ60
AM3354BZCZ100
Can you help me track this down?
Best regards,
-RT