Part Number: CC2564 Hi
We have created a product using CC2564 and we have passed certification for both FCC and CE. Now we are trying to pass the Korean radio certification but they require us to set duty cycle on a test-signal so that they can test dwell…
Part Number: CC2564MODA Other Parts Discussed in Thread: CC2564 Hello Ti-Team,
We started to develop a new Bluetooth product that works on a Man-in-the-middle concept. It should consist of two CC2564 modules, one configured as SINK other as SOURCE roles…
Part Number: CC2564 TI Support,
FYI - I am using CC2564B, not CC2564. The forum only allows CC2546 or CC2564C as a part number.
Q1: Does HCITester v3.0.0.37 work on Windows 10?
Q2: It generates an error when trying to load TIInit_6.7.16.xml script,…
Part Number: CC2564 Hi,
I want to use dual-mode Bluetooth products, CC2564RVMT/CC2564RVMR display is not recommended for the new design, is there any new product recommended now?
Could you still apply for samples? Many thanks~
Hi Furkan,
Can you explain your setup a bit more as well as explain any error codes you might receive.
Please note that the PressButton function is only available as a server to accept or end calls and not client.
Kind Regards,
Rogelio
Part Number: CC2564C Other Parts Discussed in Thread: CC2564
Hello,
Our project uses STM32+CC2564. When using iSSPdemo to communicate with mobile phones above Iphone11, CC2564 will delay sending for 20ms, as shown in the attachment:
When we receive the…
Part Number: CC2564 Hello,
We are evaluating the CC2564 for a new module. Our primary use case is SPP and iAP with low latency as our primary performance metric.
Our performance is measured by request/response per second. So, data sent from phone to radio…
Part Number: CC2564 I need the pinout of the CC2564 in the YFV BGA 54 package.
The datasheet only has the RVM VQFN-N76 package pin functions.
Best,
Steven
Part Number: CC2564 Hi,
I have old device with CC2564B, since the device is still in production I need to support it, but I can't find any help anywhere all the Wiki pages are goon, can't find any help for HCI commands.
I don't really understand…
Part Number: MSP-EXP432E401Y Other Parts Discussed in Thread: CC2564MODNEM , , CC256XCQFN-EM , CC2564 , CC2640R2F , CC2640 , CC2564CMSP432BTBLESW , MSP432E401Y
Has anyone tried connecting and running the sample applications found in the Dual-Mode Bluetooth Stack…