Part Number: DAC80508EVMDAC80508EVM do not work.
1) Power on reset.
I understand DAC80508M is used on DAC80508EVM, the DAC output (out0) initial voltage should be 1.25V, but it is near 0V at the power on.
I tried two cases of power-on as the follows…
Part Number: DAC80508EVM Can we order the evaluation board DAC80508EVM with DAC80508ZRTER or DAC80508ZRTE (zero volt output at reset).
If it's available, please, inform me the product No.
Thank you.
Part Number: DAC80508EVM The 80508EVM is connected to USB2ANY.
USB2ANY Explore works ( I done update with USB2ANY hardware ) .
Next, I run the DAC80508 Software. It is in demo mode. I try initialize, but it fails.
Please, give me advice.
Part Number: USB2ANY Dac80508evm follows "dac80508evm user's Guide". The J1 of dac80508evm board is connected with J4 of usb2any board. USB cable connects usb2any board to PC and external 5V power supply to tp6 test point of EV board. PC…
Part Number: DAC80508EVM Hello,
I am developing automated tunning procedure by using DAC80508 evaluation module. Would you provide me the LabView design files of evaluation module software? This will be very useful for me. I am using LabView 2015.
Thank…
Part Number: DAC80508EVM Hi Everyone,
Trying to get some form of comms to this DAC (DAC80508M)
The following is my SPI setup:
The MCU is an stm32f7.
The clock polarity is low and the clock phase is set to 2nd edge.
I have tried a range of clock speeds…
Part Number: DAC80508EVM
First off, I am not using USB2ANY to control the eval board, I don't have the cable. I am using an FPGA controller (CMOD A7) to connect directly to the CS, SCLK, SDI & SDO pins. I have attached a couple of oscilloscope snapshots…
Hi Mike,
Please refer to the land pattern drawings for any sizing. They are correct.
If you look at the DAC80508EVM, the footprint that is actually used is aligned with the land pattern. (screenshot from the datasheet)
The layout example likely used…
Part Number: DAC80508EVM This appears to be an Altium based design. We are designing a board now using a couple of DAC80508s and having the Altium files for a design reference would be exceedingly useful. How can we get the Altium source files for the…