Thanks for your reply! I did some experiments and found out that even after taking out the 1.8V LDO from the EVM, the 1.8V port still outputs 2.7V. For some reason, after soldering the LDO on again, the 1.8V port outputs 4.7V now, which is very weird…
Hey Sandip,
I am able to get the circuit to begin simulation analysis using PSPICE for TI; however, it cannot converge right now. See the output report. Overall, I do not see the gross netlist errors you do and software is able to begin its analysis…
Part Number: TPSM64406 Hi,
I am developing a power supply with a 12 V to 35 V input and a 5 V / 12 A output, using two linked TPSM64406 devices in a four-phase configuration.
In the attached TPSM64406 datasheet, page 19, Figure 7-4, High-Efficiency…
Part Number: AWR1642BOOST Other Parts Discussed in Thread: DCA1000EVM hi,
I am trying to mmwave SDK 3.2.0.4 for LVDS data capture using DCA1000 EVM. I have read SDK 3.2.0.4 User Guide (Product Release 3.2, Release Date : May 10, 2019, Document Version…
Der Kyle,
I was using the attached pdf to do the process.
5545.mmwave_sdk_user_guide.pdf
If there is any other white paper, can you kindly share it.
According to the attached image of page 31 of the pdf, I was flashing the highlighted bin file…
Where are the command you are sending from ?
Check mmw_sdk_user_guide to see command to send
1004.mmwave_sdk_user_guide.pdf
Did you set the DIP Switch for 40 pins connectors ?
Did you solder the resistor R81?
Mathieu
Hi Leon,
I tried to reproduce your sample video out.mp4 with the following pipeline (The one that works for me with anoter h264 encodec video in a mp4 container) and I got a Segmentation Fault error. This is the log:
=============================…