Part Number: SN65DP159 My design uses an SN65DP159RSBR to interface with a SMARC standard SBC card. On the DP side, the following signals are passed to the CPU on the SBC.
1. DP0+/- (Pins 6,7)
2. DP1+/- (Pins4,5)
3. DP2+/- (Pins1,2)
4. DP3+/- (Pins9,10)
5.…
Part Number: SN65DP159 Other Parts Discussed in Thread: DP159RGZEVM , TMDS181 Hi TI Team ,
I am intend to use the SN65DP159RGZT in my design as DP++ to HDMI ,
I was looking on the DP159RGZEVM schematics and it seems that there is a mistake in the DP159 symbol…
Part Number: DP159RGZEVM I have an issue with DP159 when setting DDC / HPD in snoop mode but no issue if DDC transits through active DDC block
1. when DDC transits through active DDC block of DP159, HDMI 2.0 source (PC graphic card) signal in ON and…
Part Number: DP159RGZEVM I just received the DP159RGZEVM and am planning to use it with the Eye Scan tool to look at the HDMI signals coming out of my design. Is there a reference guide for stuffing options to enable the HDMI input port on the DP159RGZEVM…
Part Number: DP159RGZEVM
Hello All,
SLLA358 shows below command in 4 Initial Power-up Configuration.
{0x0D, 0x02} , //Select LN0 for clock.
What exactly it means? Does it it recovers DP sink clock from LN0?
If Lane 0 is not connected then do we need to…
Part Number: DP159RGZEVM Dear all,
one of my AA is going to evaliare the device and he prefers develping e board starting from the EVM.
In order to speedup that process is it possible to have the project of the EVM (not only schematic and gerber) ?
regards…
Part Number: DP159RGZEVM Hello All,
Q.1. Is it possible to reduce no of lanes of DP159 on hardware schematic for DisplayPort Application? By default this connection is 4 lanes, we want to reduce it to two lanes.
Q.2. If yes, does clock lane connection…
Part Number: DP159RGZEVM Other Parts Discussed in Thread: TUSB1064RNQEVM Hi,
I am planning to use DP159RGZ Evaluation Module in order to convert DP signal to HDMI.
When I connect the board to a monitor (HDMI in) and a PC (DP out), it works out of the…