Part Number: DP83869HMDP83869HMRGZT: MDI interface between PHY and 88E6321 Marvell switch.
Hi,
If the Ethernet switch (88E6321) is connected to the TI PHY (DP83869HMRGZT) via MDI lines and both devices are on a single PCB in an enclosed local system…
Part Number: DP83869HM holla,
Can you configure the DP83869HM as a media converter only via a pin strapping? Application: RJ45/1000BASE-T <- -> 1000 BASE-X/SFP The information I have read is contradictory.
best regards
Martin
Hi Sanju,
Glad to hear everything is okay on PC end.
Please share the schematic with me so I may review (email to e-mayhew@ti.com for private share).
Also, please confirm if there are any differences in the current register dump values relative to the…
Hi Toshikazu,
Thank you for clarifying the research you are working on.
Although we have seen DP83867/869 in ECAT applications, loopback is not typically used beyond the evaluation/troubleshooting stage.
As a result, we do not not have the data readily…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869 To whom it may concern -
What is the time synchronization precision range for the DP83869? Is it capable to reach the 100ns range?
Thank you.
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869EVM , DP83869 Hi,
I experiece some link stability issues with the DP83869HM with some link partners.
The DP83869HM is operated in 1000-Base-X media converter mode.
I have seen this on our hardware…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869 I am trying to get the DP83869HM to output a pulse to the MAC during both Tx/Rx for SFD.
Do I just have to set the following to get it to work?
Register: GPIO_MUX_CTRL Offset: 1E0h Field: LE…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869 Hello Support team,
For I210 IT(COPPER) to DP83869(FIBER) application, how to set the indicating LED(1G/100M/Link)?
(DP83869: LED_0, LED_1, LED_2 PINs)
Thanks.
Best Regards, Dave