Part Number: DS250DF410 Hi Team,
If would like to use DS250DF410 support 1.25Gbps data rate, is follow the step as below E2E thread show can also achieve it? Since it looks like only change to bypass mode.
https://e2e.ti.com/support/interface-group/interface…
Part Number: DS250DF410 1. Does a QSFP28 100G port use 2 pieces of DS250DF410, and one piece (schematic bit U68) of CAL-CLK-OUT must be connected to the other piece (schematic bit U70) of CAL-CLK-IN? Or can we provide separate clocks for the two chips…
Part Number: DS250DF410 Other Parts Discussed in Thread: DS560MB410 , DS280BR820 , , DS250DF230 Hi,
I am current working on a project where I need to have a 25G interface between an FPGA and SFP28 module. The trace length is coming around 7.5 inches with…
Hi Jay,
JAY Lee said: 1. Our ASIC only support SFI, no KR. So the loss criteria is more critical than our thinking before.
What is the channel loss in your system? Can you add this to your block diagram?
JAY Lee said: 2. We’d like to know about re-timer…
Part Number: DS250DF410 Hi Expert,
My customer use DS250DF410 and setting the data rate as 10.3125GHz now.(Setting 0x2F to 00) But they would like to increase the data rate slightly +25ppm.
May I know can DS250DF410 increase the data rate +25ppm when…
Hi Allan,
I have not seen this device implemented in an Ethernet system before. HD3SS3212 might work, but is not able to apply any equalization to the signal. This might be challenging for a front port application.
You might also consider DS560MB410, which…
Part Number: DS250DF410 Hi Expert,
Pls help to review the schematic design.
End customer: Delta
Applicant : 800G switch
Core chip: TAMAHAWK 5 chip to support 2 ports SFP28
Pls see the attached schematic design.
delta_DS250DF410ABMR.pdf
Thanks
Eric
Part Number: DS250DF410 Hi, TI support team
I have an inquiry regarding a project that our client is currently planning.
I would like to share the block diagram received from the customer and contact you via e-mail, so please let me know your email address…
Part Number: DS250DF410 Hi Expert,
my customer is using DS250DF410 in EE Switch, we meet a crosspoint function failed issue now.
issue description: crosspoint mode failed but CDR is locked, 0x78 is 0x30
test we did:
for the straight mode, CDR could…