Part Number: DS90CR286A-Q1 Hi expert,
The maximum power supply current of this chip, if I use Pclk within 40M, the output is 70mA.
What is this 70mA current? Does it mean that the maximum total current of VCC1, VCC2, VCC3, VCC4, LVDS-VCC, and PLL-VCC…
Part Number: DS90CR286A-Q1 Other Parts Discussed in Thread: SN65LVDS822 Hi, Support Team
DS90CR286A-Q1 can support LVDS clock 8MHz frequency?
Our spec: LCD DCLK frequency 8~12MHz requirement.(LVDS to RGB888)
if any suggestion, Please advise me.
Thanks…
Part Number: DS90CR286A-Q1 Other Parts Discussed in Thread: DS90CF384A , SN65LVDS822 Hi Team,
Because DS90CR286AQMT & DS90CF384A out of stock
RD is looking for other replacement
>>Please help suggest IC
SPEC:
The current image source output is LVDS…
Part Number: DS90CR286A-Q1 Hi team,
customer would like use DS90CR286A-Q1 to drive a 1.8'' TFT, below is TFT spec.
but the min PCLK of DS90CR286A-Q1 is 20MHz, which is higher than TFT clock. do you have other recommendations for this application…
Part Number: DS90CR286A-Q1 Hi Team.
In order to obtain better EMI performance, how to connect the three grounds LVDS_GND, PLL_GND and GND? Thanks.
Best regards,
Ansel Song
Part Number: DS90CR286A-Q1 Other Parts Discussed in Thread: DS90CR286 , DS90CR286AT-Q1 , Hello, Does DS90CR286 support BT.601 or BT656? Are the BT.601 or BT656 just a parallel interface?
also please tell me difference between DS90CR286A-Q1 and DS90CR286AT…
Other Parts Discussed in Thread: DS90CR286A-Q1 , SN65DSI83-Q1 , DS90UB941AS-Q1 Hi team
My customer has requirement (with AECQ100) for MIPI DSI to RGB conversion.
Is SN65DSI83-Q1 + DS90CR286A-Q1 a suitable pair, if customer need AECQ100 parts for converting…
Hey Bryan,
It looks like there is no PSpice model that was developed. There is an IBIS model for the DS90CR286AT which can be used for the DS90CR286A as well: https://www.ti.com/product/DS90CR286AT-Q1
Thanks, Lysny
Part Number: SN65LVDS822 Other Parts Discussed in Thread: DS90CR286AT-Q1 , DS90CR286A-Q1 , SN65LVDS86A-Q1 Hi all
My customer has a design with the SN65LVDS822.
Because of the constrained market they are looking for a potential replacement option.
Is there…
Part Number: DS90CR286A Other Parts Discussed in Thread: SN65DSI84 , , DS90UB941AS-Q1 Hello,
It is planned to use for long-term project solution based on SN65DSI84 + DS90CR286A.
Are these parts recommended for new designs for long-term production?
Can…