Part Number: LM96063 Other Parts Discussed in Thread: AMC80 , LM96080 , LM96194 , LM94 , LM96000 , LM93 Hi,
We currently have a project for the Intel Q670 platform. We have a total of 4 fans (2x SMART FAN and 2x non-Smart 12V FAN). However, due to the limited…
Part Number: AMC6821 Other Parts Discussed in Thread: LM96194 , LM96000 , LM93 Hi Sir,
We would like to find FAN speed controller solutions(I2C interface, up to 6-CH is better).
May I have your recommendation on this?
Thank you.
Hi Michel,
Please look at the LM96000, LM93/LM94 or LM96194 datasheets and see if these one of these will work for you. These devices have two remote temperature sensors and should not need calibration with the recommended junctions mentioned in the…
Part Number: AMC6821 Other Parts Discussed in Thread: LM96000 , LM93 I have a customer in need of a fan controller similar to the AMC6821, but preferably a dual version.
The sensor will be off the board--maybe 18” away. Will need a cable.
How accurate…
Hi Nimesh,
I was able to replicate the variation of the PWM duty cycle. This variation is a result of using High resolution mode (register 0x45 bit:4 =1). For more consistent PWM use standard set register 0x45 bit:4 =0.
Also below is my feedback on your…
Part Number: AMC6821 Other Parts Discussed in Thread: LM96194 , LM94 , LM96000 , LM93 Dear Team,
Can you help on suggesting the suitable device for my customer?
Input : FAN’s present x4 or x8
Input : FAN’s TACH x4 or x8
Input : Thermal interrupt…