Part Number: LMK04816 Other Parts Discussed in Thread: ADS5400 , DAC5682Z , , LMK04828
Hi Team,
I develop board with 10 x DAC5682Z & 2 x ADS5400.
I looking for clocking solution, I saw LMK04816/28 but it will be great if you can suggest your recommendation…
Part Number: LMK04816 Other Parts Discussed in Thread: PLLATINUMSIM-SW From LMK04816 datasheet:
1. PLL1 typically uses a narrow loop bandwidth (10 to 200 Hz) to:
- retain frequency accuracy of external reference clock
- suppress high offset frequency…
Part Number: LMK04816 I tried the following methods: 1. Use power divider to connect input clock to CLKin1 (FBCLKin) and CLKin0. Use 0 delay mode, and choose FBCLKin as feed back. The result is that the output clock can be synchronized with the input…
Hello Alan,
The phase transfer functions (open-loop and closed-loop) will be different when the loop is closed outside first synthesizer (VCO2 output to PLL1) from when the loop is closed from VCO1 to PLL1.
For example, taking clock reference input…
Part Number: LMK04816BEVAL Other Parts Discussed in Thread: LMK04816 I have a LMK04816 Eval board from which I am trying to get 125 MHz and 6.25 MHz clock signals. I have a 50 MHz clock signal that I can bring onto the board. The board is equipped with…
Part Number: LMK04816 Other Parts Discussed in Thread: CODELOADER Hi All.
I'm using the LMX04816 Eval Board with PC -- LPT-uWire cable.
When I try to select in 'Select Device' LMX04816 CodeLoader display Run-time error '13' and shut down.
I use…
Part Number: LMK04816 The board designed by ourselves, the same output circuit design and the same LDO provide 3.3V power supply for vcc_clkout.
Using software to configure the same frequency output frequency (2.4 GHz) and the same level standard (LVPECL…
Part Number: LMK04816 Hi,
Regarding the programming of 32 registers of LMK04816, is it performed after each register is written or after all registers are written?
If two outputs are placed in two different GROUP (switch bits in different registers…
Part Number: LMK04816 Hi,
Regarding the programming of 32 registers of LMK04816, is it performed after each register is written or after all registers are written?
If two outputs are placed in two different GROUP (switch bits in different registers…