Other Parts Discussed in Thread: LMP91000EVM , MSP430FR5969 , LMP91000 Hello,
I'm attempting to interface the MSP430FR5969 microcontroller with the LMP91000EVM potentiostat via i2c communication. I've been troubleshooting the main.c code in code composer…
Other Parts Discussed in Thread: LMP91000 , LMP91050 , LMP90100 Hi to all,
I'm using the LMP91000 and I can't find the Methane sensor in the software. Do I have to configure the soft to use the methane sensor ?
Regards
Gastón
Hi Marie,
There are no LabVIEW drivers that I am aware of that will directly control the LMP91000 on the SPIO-4 board. Can you expand on your comment about the LMP91000 v1.1.06 software? What is it about the SW that does not meet your needs? There is…
Other Parts Discussed in Thread: LMP91200 , LMP91000 Hi
I am already thinking about using the LMP91200 for the pH sensor interface and trying to find something that can be used with MT dissolved oxygen probes. I am using the 6000i series. I think the…
Hi Alejandro,
with 2.5V of VREF the max bias you can reach is 600mV (24% of VREF).
Even if you supply the LMP91000 with 5V and you connect a 4.096V voltage reference, the max bias will be 980mV.
1600mV can be reached only with a voltage reference…
At present, there is such a part, eletrochemical analog front end plus ADC but LMP91000. my suggestion is to consider LMP91000 + MSP430F2013 / MSP430AFE251.
wish it helps.
Best regards
Hawk
Other Parts Discussed in Thread: LMP91000 , LMP90100 Hello, I am trying to evaluate the performance explosive sensor
http://www.sgxsensortech.com/site/wp-content/uploads/2012/10/VQ548ZDW.pdf
have the module lmp91000 but it cant use these sensors…
Other Parts Discussed in Thread: LMP91002 , LMP91000 Hi there,
Can you guys recommend some electrochemical CO sensors for LMP91002, I don't know much about the sensor manufactures.
Hello Nick,
the LMP91000 when supplied at 5V, and configured in order to use the supply as internal source of Voltage Reference is able to generate a maximum differential voltage between RE and WE pin which is 24% of the Voltage Reference, in this…