Part Number: MSP-EXP430FR6989 I am having a little bit of trouble finishing this code, I need to make the LED's blink, not mattering the order, I think I am messing up the configuration.
;----------------------------------------------------------…
Part Number: MSP-EXP430FR6989
Hi, i got a TI LauchPad and i tryed to run a code to check if the leds on the board turned on. But it does not
I all ready test to code on a other Pad from a school budy and the code runs fine
I think…
Part Number: MSP-EXP430FR6989 Other Parts Discussed in Thread: CCSTUDIO Hi Team, seeking for some support.
According to our customer, the UART seems not functioning there board. Here are the details step that they performed.
Hookup Steps": 1) Plug…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: MSP-EXP430FR6989
Hi all,
I tried to test firmware TIDM-3LC-WATERMTR with kit MSP-EXP430FR6989. But when i tried to test, the signal from ESICH0, ESICH1, ESICH2 was very strange. I use coil 100uH…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: MSP-EXP430FR6989 Hi all,
I tried to test the LC sensor with kit MSP-EXP430FR6989, it works well at room temperature, but when I tested it at above 60 o C, it was wrong (the value is less than the…
Thanks for looking into the matter.
Eason Zhou said: difference between you can flash the device and can't flash the device
"can flash" means I can run a debug session on board to start/pause/stop the logic for debugging using CCS.
"can't…
Part Number: MSP-EXP430FR6989 Hello
I have some issues while debugging with that launchpad or rather it's related to CCS I think. Sometimes I cannot debug or run firmware on launchpad until I restart CCS. In debug window there is no any active debug sessions…
Part Number: MSP-EXP430FR6989
I am trying to develop a program to read DHT-11 sensor from the bottom up. For this reason, I need to use Timer in capture mode.
1. P1.3 is selected for capture input. I want to capture on the falling edges. But I could…
Maynard,
Unfortunately, I'm out of work arounds for the customer. I'm not sure why their eZ-FET can communicate with the PC but successfully update. This is not behavior that is typically seen so at this point, I'd just going to assume that some…
Part Number: MSP-EXP430FR6989 Other Parts Discussed in Thread: LAUNCHXL-F28379D , Hi Team, Do we have a device in the MSP430 portfolio that supports LTE and can be integrated with an LTE module? Our customer currently has the MSP-EXP430FR6989 and LAUNCHXL…