Hi,
in case you are using the 38 pin TSSOP package, you can buy the development kit and the USB programmer bundle:
http://www.ti.com/tool/msp-fet430u38
otherwise you need to build your own custom board and add the JTAG connection pinout:
http://processors…
The MSP-TS430DA38 board is a socketed EVM specifically designed for evaluating F2272/4 parts. As Leo mentioned, you'll need an MSP-FET430UIF programmer. If you don't already have one, you can get the MSP-FET430U38 kit, which includes both the MSP-TS430DA38…
Dear,
I've questions as below urgently?
1. I'd like to use LPM3 that is used VLOCLK only.
is there a way that VLOCLK can be corrected with F/W code?
in other words, Is there a way to compensate for VLOCLK with F/W code ?
2. Can I use TIMER1,…
Hi 78Sys,
The MSP430G2955 is actually a pretty new part, I think it only came out in the last year. The EVM that can be used is linked off of the MSP430G2955 product page, and I've also provided the link here. This is kit with FET tool for programming…
Other Parts Discussed in Thread: MSP430F2274 , MSP430WARE , MAX232 Hi, I am new to msp430 programming and have a msp-fet430u38 kit with a msp430F2274 chip. I am using msp430Ware and running the samples. I can get the Led sample to work, but not the msp430x22x4_uscia0_uart_01_9600…
Hi Vikram,
The G2xx5 parts have at least 38 pins and will not fit on the Launchpad, and they are not supported by the Launchpad's programming interface.
You will need the Target board kit that you linked and an MSP-FET430UIF tool - there is a version…
Hi Joseph,
I think that the firmware in the MSP-EXP430G2 Launchpad on-board eZ430 programmer does not include support for the G2955 device. This part is very new, and as it does not even fit on the MSP-EXP430G2 Launchpad the eZ430 programmer firmware likely…
Howard Tang said:
I need to buy a MSP430 and it will be mounted on PCB with my power management unit, which type of packaging should I buy?
You will need to select the ideal MSP430 for your application based on your requirements. You will know these…