Other Parts Discussed in Thread: CC2340R5 , MSP430F6638 Hello,
We are exploring the CC2340R5 BLE module. We want to connect this BLE module with MSP430F6638 microcontroller via UART.
Can you help us with the reference code for MSP430 to communicate with…
Part Number: MSP430F6638 Other Parts Discussed in Thread: MSP430FR4133 , MSP430FR4131 Hello, We are exploring MSP430F6659IPZ and MSP430F6638IPZ microcontrollers. We need to interface a custom 148-segmented LCD with a microcontroller which I have attached…
Part Number: MSP430F6638 I have partioned my main memory into bootloader and Application area. Want try to move interrupt Vector to RAM to execute bootloader with interrupt as smooth and crisp as possible.
I've searched around for real life simpel examples…
Part Number: MSP430F6638 Hey,
Do anybody have complete sample code or link to sample code showing how to enable PU.0 and PU.1 as Output pins and toggle them High-Low.
I am aware of section 42.2.1.3 Port U Control in the MSP430x6xx Family Users Guide…
Part Number: MSP430F6638
Hi,
I am trying to get my MSP430F6638 to work with Linear Technologies AD7780 which is an ADC. The ADC communicates via a 2 wire SPI connection. I realized when setting up the MSP, it would only allow me to configure the MSP…
Part Number: MSP430F6638 I have a 1V dc level applied to an op-amp buffer. The output is then feed through a 1kohm/1kohm voltage divider and then feed to to ADC0 input of the MSP430F3368. Instead of reading 0.5V I get a reading equivalent to 0.7V . When…
Part Number: MSP430F6638 Hi, there
i am trying to use TI-RTOS on MSP430F6638. but i am not able to use TI-RTOS on msp430. for this specific controller is it supported because i am not able to find out any examples. can i get help on this topic.
Part Number: MSP430F6638 Hello Support Team,
Hello Support Team,
I am using MSP430F6638IPZ in my current project. I have a query regarding this. I have a soldered Controller, Decoupling capacitor, 2-wire JTAG, and crystal on my board. I have give external…