Part Number: MSP430FR6045 hello. everyone
I am currently building and testing a custom board using the MSP430FR6045.
I have additional questions. If you look at the USS Demo Source, g_ResultsOfLastMeasurement.last_volume is declared as float type. So, when…
Part Number: MSP430FR6045 I am testing the test with five custom PCB which use MSP430FR6045.
And I use external 32.768kHz x-tal.
I put the actual time into the RTC module and started the time passed test.
When I check the time after 62 hours, time passed…
Part Number: MSP430FR6045
Development is in progress using MSP430FR6045. The source is being developed based on the USS_Water_Demo source provided by TI.
Sometimes the operation stops with "Break at address "0x39b5c" with no debug information available…
Part Number: MSP430FR6045 USS_water_demosdk is testing UART.
It was connected to pin 0, 1 of port 7 of MCU by TTL module from PC. (eUSCI_A2 module) EUSCI_A's Uart Clock Source is using SMCLK(8MHz, HFXT).
When the baud rate was 115200 and gHMI.isLPMenabled…
Part Number: MSP430FR6045 After making custom boards and pipes using msp430fr6045, calibration is in progress.
I have a question regarding this.
1. How to calibrate the flow rate using the total volume In USS, it proceeds in VFR Flow of Calibration tab…
HI,
Oh, okay. It should depends on the flow rate range of your meter. Kind of related to the diameter of the pipe.
We do not have a recommend data either. If your flow rate range is 25LPM to 40000LPM for a DN25 pipe for example. You might need to measurement…
Part Number: MSP430FR6045 Other Parts Discussed in Thread: MSP430FR6047 MSP430FR6045 custom board is being produced and developed. When PC, Cativate, Custom Board are connected and USS Tool is connected, the message “HID Bridge Connected -- waiting for…
Part Number: MSP430FR6045 Other Parts Discussed in Thread: MSP430FR6047 Hi,
I'm testing USS_Water_Demo project.
I use the MSP430FR6045, so I changed the device setting from FR6047 to FR6045 in project properties.
Also, I modified lnk_msp430fr6045.…
Part Number: EVM430-FR6047 Other Parts Discussed in Thread: MSP430FR6047 , MSP430FR6043 , MSP430FR6005 , MSP430FR6007 , MSP430FR6045 , MSP430FR5043
Hi
My customer is asking why smart water meters we are using MSP430FR6047 and Smart Gas Meters we are using…
Part Number: CAPTIVATE-PGMR Other Parts Discussed in Thread: MSP430FR6045 , , EVM430-FR6047 MSP430FR6045 Custom Board is being tested by connecting it to the USS program.
The PC and custom board were connected using CAPTIVATE-PGMR. At some point while using…