Part Number: MSP430FR6820 Other Parts Discussed in Thread: MSP430FR68221 , , MSP-FET Hi Team,
could you indicate how much time/seconds does it take to program 60KB FRAM memory by the I2C BSL in MSP430FR6820IG56R?
It would be perfect to have a table for…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…