Part Number: MSP432P4011T On MSP432P4011T I want to generate PWM signals and communicate via Uart at same time, but when the pwm is initialised the uart communication fails. My uart pins are p1.2 and p1.3 and my PWM pins are P7.1 and P7.2 .
my code segment…
Part Number: MSP432P4011T Tool/software: Code Composer Studio Hi, now I'm debugging my MSP432P4011TRGCT custom board, with using MSP-FET.
Within debugging, connection error has happened.
The error message is "CORTEX_M4_0: Error connecting to the target…
Part Number: MSP432P4011T I was working with MSP432P4011T and was trying it to program it for the first time. According to my understanding if the controller is not programmed it will be in its BSL section and we just need to run the BSL application from…
Part Number: MSP432P4011T I am working on MSP432P4011T microcontroller and want to communicate with the controller over pcie smbus. Does MSP432P4011T support PLDM over mctp? Is any support or software stack available for the same?
Part Number: MSP432P4011T I am working on MSP432P4011T microcontroller and want to communicate with the controller over pcie smbus. I tried to configure my BMC as slave as follows:-
#define SLAVE_ADDRESS 0x48
MAP_GPIO_setAsPeripheralModuleFunctionInputPin…
Part Number: MSP432P4011T Hi,
We are planning to use MSP432P4011TRGCT in one of our project. But datasheet doesn't provide package land pattern & assembly details of RGC 64
This data is missing even in http://www.ti.com/packaging/docs/searchtipackages…
Part Number: MSP432P4011T Hi,
I have done pin assigning in PIN-MUX tool. I need three set of I2C. When i select three I2C. Two sets are assigned correctly. One set is assigned to PIN 13 and PIN 14.
When I check the datasheet. These pins doesnt have I2C…
Part Number: MSP432P4011T Hi, I am working with MSP432P4011T. In my design i need three I2C and thirty six GPIO pins. By using pin muxing tool when i added 3 I2C, one among them was assigned pin numbers 13 and 14. But when i checked in the datasheet ,…
Thanks, Angelo.
Wiki page helps to solve my doubts about how to initialize all unused ports.
Still, I have a doubt on hardware pin out when I check the datasheet and pins of my controller PORT 10 and some other ports are not available on hardware pins…