Part Number: SN65LVDS33 Hi Sirs, Can the SN65LVDS33PW convert differential signal of eDP AUX (1Mbps) to 3.3V single-ended output? If not, would you please a proven solution? Wayne Chen 11/03/2023
Part Number: SN65LVDS33
We have added external series resistor of 25ohms to the out pins(Y) of SN65LVDS33 for maintaining 50ohm impedance,
Do you have any Layout guidelines on placement of resistors
Part Number: SN65LVDS33-EP Hello,
For the SN65LVDS33MDREP, the only “operating factor” of 7.6mW/C is given (which I in turn calculate 131.6C/W for theta-JA). Do you have unpublished theta-JC and theta-JB?
Thanks,
Adam
Part Number: SN65LVDS33 Other Parts Discussed in Thread: SN65LVDS31 , Hi
If you have any IBIS model of the SN65LVDS33 and of the SN65LVDS31 LVDS XCVR, please send me, no matter the exact packaging
Thanks
Amnon
Part Number: SN65LVDS33 Other Parts Discussed in Thread: SN65LVDS31 , Hi
Can you send me please the SN65LVDS33PW and SN65LVDS31PW IBIS files?
I failed to find them on your WEB
Thanks
Amnon
Part Number: SN65LVDS33 Other Parts Discussed in Thread: SN65LVDS31-33EVM Hi,
I am working with Laurier and Aki on the linked issue.
In summary, we are trying to use the SN65LVDS33 to receive qty two 100 MHz clock signals (when I say 100 MHz, I mean a…
Part Number: SN65LVDS33 Other Parts Discussed in Thread: SN74AUP1G34 , SN74LVC1G34
Hi Team, seeking some help.
The load resistors are set so IOH/IOL doesn't exceed +/-1mA at maximum output voltages. The key is CC compensation capacitor. Ideally R1 x CC…
Hi Malik,
Malik Barton57 said: Have you also measured the jitter in the LVDS side in the same way?
Yes, we measured it. It is essentially null
Malik Barton57 said: Are you seeing the jitter issue on the data pins as well
Yes, but it is less pronounced…