Part Number: SN75LVCP600S Tool/software: SN75LVCP600S data sheet states "Operating free-air temperature" from -40C to +85C.
Question:
Operating free-air temperature is a vague term. Most TI data sheets, tells us the Max Operating Jc.
Can you…
Part Number: SN75LVCP600S Tool/software: Background: We are using about (6) of these devices on one of our product's. Running SATA at 6Gbps. At room temp. file transfers work fine using FileZilla.
When we operate at -30C, once in a while we loss…
Part Number: SN75LVCP600S Hello,
We are experiencing some issue with this schematic :
It works well with SATA Gen2 3Gbps but a lot of errors in SATA Gen3 6Gbps. This PCB is placed between a ComExpress board and a SATA SSD (cable + rack).
I now there is…
Part Number: SN75LVCP600S Other Parts Discussed in Thread: DS64BR111
Hello Team,
I am working on SATA interface with data rate of 6 Gbps. In the Ti portal i am able to get Hspice model. Since I am using HyperLynx tool for simulation. Hspice model is…
Part Number: SN75LVCP600S Can SN75LVCP600S be used normally under linux? Because I have seen in other materials that SN75LVCP600S cannot recognize and read data under the Linux system, are there any successful application cases under the Linux system …
Hi Aiwen,
SN75LVCP600S is controlled pin settings. Based on your comments, i believe pins EQ(pin5) and DE(pin 9) needs to be tuned. If these tuning of these two signals do not help, then we may need to set SQ_TH(pin 10) appropriately. Please setup scope…