Part Number: TCAN1042DEVM Tool/software: Hello, Team,
Can we get a BOM list of TCAN1042DEVM? It is not included in the user guide pdf.
Best Regards, Masaru
Part Number: TCAN1042DEVM Tool/software: Hello, The EVM has C3 and C5, though they are DNI. Under what circumstances should they be populated? And under the circumstances that C3 and C5 are required, how can users determine the values of C3 and C5 respectively…
Part Number: TCAN1042DEVM Hi, I am trying to establish MCAN external loopback communication. My setup includes a AM62A, connected to the TCAN, which is connected to a PCAN module, and the data can be viewed on PCAN view software. The connections for TCAN…
Part Number: TMS320F28379D Other Parts Discussed in Thread: TCAN1042DEVM HI,
I want to use CAN channels on the F28379D board. I am looking for CAN transceivers that are compatible with this board. I found this board, TCAN1042DEVM, that may help me. Please…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: TCAN1042DEVM I was wondering how I can configure the LAUNCHXL-F28379D to use the TCAN1042DEVM as the second CAN transceiver. For my system I am wanting two CAN interfaces to talk with different…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: TCAN1042DEVM
I was wondering how I can configure the LAUNCHXL-F28379D to use the TCAN1042DEVM as the second CAN transceiver.
Part Number: TCAN1042DEVM I am working on CAN communication and I have come across a CAN database (.dbc) file which has one message which contains signals with both, intel & motorola byte order (Like Case 1, 2 & 3 metioned below). So I implemented a logic…
Part Number: TCAN1042DEVM Dear TI Support,
I have two question about this TCAN1042DEVM,
1. If I want to test a start topology can bus with 6 nodes. each one with less than 20" wire. is there a software provided by TI that can serve is a Master node?…
Part Number: TCAN1042DEVM Other Parts Discussed in Thread: TCAN1044A-Q1 , TCAN1042G-Q1 , TCAN1042GV-Q1 Hi,
I have a TCAN1042EVM but it has TCAN1042Q1 which supports a max CANFD bitrate of 2Mbps.
My requirement is 5Mbps CANFD datarate. And this is offered…
Part Number: TCAN1042DEVM Other Parts Discussed in Thread: TCAN1042V-Q1 , TCAN1044AV-Q1 Hi there,
So what is the default device on the TCAN1042DEVM?
If I want to use EVM with 3.3V VIO, should I replace the device with TCAN1042V-Q1?
Thanks,
Yuhao