Part Number: TCAN4551-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 Hi there,
Would there happen to be an IBIS or PSPICE model for this part?
Thank you,
Ekko
Part Number: TCAN4551-Q1 Other Parts Discussed in Thread: TCAN4550-Q1 Hi team,
When doing a schematic review for a customer, I noticed that they have the SJA1000 designed in, but it looks like it is obsolete according to Mouser. In this vein, I thought…
Part Number: TCAN4551-Q1 I am currently using watermark interrupt to read FIFO. I have it set at 48. Things seem to be working fine.
However, I am thinking of a case where there might be some data in the FIFO at the end(of transmission/or during network…
Part Number: TCAN4551-Q1 Hello!
I am seeing that after running for sometime, Rx FIFO0 status register shows RX FIFO0 full status.
To see exactly what is going on, I started reading the FIFO0 status register every 1 second and I noticed that just before…
Part Number: TCAN4551-Q1 Hello, I think max 18MHz SPI clock is recommended for 8Mbps data rate operation. Do you have any data for how much bit rate can be realized with other SPI clock rate? Do you have a kind of table that show CAN bit rate V.S SPI clock…
Part Number: TCAN4550
Dear TI,
which interrupts are represented by MCAN_INT_0 and MCAN_INT_1 lines,
pls share if any document available, i have'nt found it in SLLU270(TCAN45xx Software User's Guide) and datasheet
i need to set either GPIO0 or…
Part Number: TCAN4551-Q1 Where can i find Linux drivers for TCAN4551-Q1 / TCAN-4550? Is the driver part of Linux Mainline? https://elixir.bootlin.com/linux/v6.6.3/source/drivers/net/can/m_can/tcan4x5x-core.c
Part Number: TCAN4551-Q1 Other Parts Discussed in Thread: TCAN4550 , Hello team,
Can I pull down nCS pin to the GND? There is no other slave device connected parallel to TCAN4551.
If I can, what would be the size of the pulldown resistor?
Best Regards, Kei…
Part Number: TCAN4551-Q1 Hello team,
According to the datasheet, there is weak pull up on the SCLK pin. However, I want SCLK to be LOW, when CPU start up.
What is the resistor value I need to pull down in order to cancel the weak pull up?
Best Regards…
Part Number: TCAN4551-Q1 Other Parts Discussed in Thread: TCAN4550 Hi team,
My customer has a design with TCAN4551 and they has trouble to wake up the device, could you help comments below questions:
1. device ID
The device ID the read out is not aligned…