Part Number: THS1206 Hi,
I am working on THS1206 ADC interfaced to FPGA (XC7A75TFGG676-2L). The 2 control registers programmed as: CNTR0 = 0x0C8 and CNTR1 = 0x410. When I am reading the data from the ADC for both the channels data out is same. The 2 inputs…
Part Number: THS1206
While investigating the alternatives to replace THS1206, I now notice that a new datasheet has been published (on the 6 th of April), where the THS1206 is placed as ‘active’ ?
What is going on with this device?
In December…
Part Number: THS1206 Hello,
Recently we received the notice that THS1206IDA will be obsolete soon, so we are checking the replacement for this part.
We found that THS1206QDA is still active and with extended operating temperature range, but the tolerance…
Hi Tom,
I do agree and I had programmed DATA_AV as lo, pulse.
Registers configured as: CR0 = 0x020, CR1 = 0x410. I will add logic analyzer results in next mail since my board is unavailable.
Regards
Part Number: THS1206-EP Other Parts Discussed in Thread: ASH , THS1206M , THS1206
Hi ,
Is THS1206-EP space qualified part ?
Is it RAD tolerant or RAD Hard ? or it is just enhanced part!
Thanks
Ash
Part Number: THS1206 Other Parts Discussed in Thread: TL431 , TLA431 Dear Team,
My automotive customer is using THS1206 in a project and has some questions. Thank you in advance for your support.
They decided to place a external voltage references (3.5V…
Part Number: THS1206 Dear Team,
My customer has the following inquiry regarding THS1206 voltage reference tolerances, I hope that you will be able to answer:
The reference voltages have large tolerances in the datasheet (VREFP= 3.5V (+/-0.2V) and VREFM…
Part Number: THS1206 The data sheet for the THS1206 (SLAS217H) states that bit 1 of Control Register 1 has a dual purpose:
a. In read mode it is the overflow flag (OVFL).
b. In write mode it is FIFO Reset (FRST).
However, I cannot figure out how to…
Hello. Peter,
In the previous poster, I was about the source code for the MCU (MSP430F449IPZ).
That's why I asked the MSP430 forum.
It seems to be a notice of a partial decision.
Again, I ask sequential questions to the link address of the previous…
Part Number: THS1206 Hello,
Could you please provide more details on sizing the inductor and capacitor filter on AVdd and BVdd from the user's guide? http://www.ti.com/lit/ug/slvu098/slvu098.pdf
The BOM calls out a 15uH CTDS1608C-153.
Is there a ripple…