Part Number: TIDA-00630 The unit received does not function.
Tested:
- on 3 different host devices (Windows 10): HP Zbook Studio, Dell Inspiron, Microsoft surface Pro 7
- with 4 different USC-C cables (all functional with other devices)
- all cases both…
Part Number: TIDA-00630 Hi all,
I have a customer-selected Qualcomm SOM with only one USB 3.1 superspeed interface. According to SOM datasheet it is possible to use USB for output as Displayport 4k@60Hz.
SOM also has pins DP_USBC_ORIEN and DP_AUX_EN_N…
Part Number: TIDA-00630 Hi!
Will TIDA-00630 will work for Android Tablets?
https://www.ti.com/tool/TIDA-00630
Android tablets usually become Accessory when connected to charging.
I wonder if this TIDA-00630 approach Android Tablet will still see devices…
Part Number: TIDA-00630 Hi Team,
I am going to built-in a type-c dock in one of my product. Looks like that TIDA-00630 is a good choice. There are some unclear that i would like to ask:
1. Can it reach 4K at 60HZ when it connected to a Mini Displayport…
Part Number: TIDA-00630 Hello! I am working with the TIDA-00630 reference design to design my own USB type c hub using TI hardware.
In the reference i saw the the CRX1N from the type c UFP is connected to CRX1P on the MUX and vice versa.
Should it be that…
Part Number: TIDA-00630
Hi Team, I found the following USB Type-C Dock Reference Design. http://www.ti.com/tool/TIDA-00630?keyMatch=TIDA-00630&tisearch=Search-EN
My customer considers to use TUSB8041 and one of four port to be Type-C connector for his…
Hello Team,
As shown in TIDA-00630 TI Type-C Dock , the both Type C port is DFP(source only), And USB 3.0 Type A is UFP.
Now the question:
1. Could we connect simultaneously two type C source one for power and other one for communication with USB3.0 Type…