Other Parts Discussed in Thread: TIDA-00987 TI Developed for production by others the TIDA-00987.
www.ti.com/.../TIDA-00987
Can any one assit where can I order 10Units?
Thank you, Aharon
Hi Hope,
I work with Shlomi on this project and I would like to make sure there are no misunderstanding with regards to desired functionality of this board...
Below attached a block diagram of the desired system.
We would like to charge the phone, at…
Part Number: LM53635-Q1 Other Parts Discussed in Thread: TIDA-00987 Hi Team,
1. Can TPS53635 passed CISPR25 level 5 without spear spectrum function?
2. What is the side-effect of spear spectrum function? Eff? anything else?
Thank you.
Part Number: TPS25810-Q1 Other Parts Discussed in Thread: TIDA-00987 , TPS25810 Hi
I would like to design automotive media port. So I interest in reference design TIDA-00987.
And I have a question.
If i set TPS254900 to client mode (CTL1=0,CTL2=0). OUT…
Hello,
It depends on how much power you are wanting to supply. If you want to supply up to 15W of power (5V/3A) I would recommend using the TPS25810. Here is a reference design that you can follow which implements a Type-C charging as well as USB3.0…
Other Parts Discussed in Thread: TPS2549 according to the TIDESIGN OF http://www.ti.com.cn/tool/cn/TIDA-00987?keyMatch=TPS25810&tisearch=tidesigns
Wandering What is the difference between TPS2549 and TPS254900,why TI design choose TPS254900 instead of…
Hi Shlomi,
In that case, I would recommend using the TPS25810. The TPS25741 is a PD controller, and since you are not using any alternate modes or not exceeding 5V, there is not need to use it. The TPS25810 is a Type-C controller that is capable of controlling…