Part Number: TIDA-010083 Other Parts Discussed in Thread: TPS23758
Tool/software:
Hello,
As per design guide TIDA-010083, The Auxiliary input voltage is designed for 18V to 36V, is this can be changed to 10V to 36V Auxiliary input voltage and what will…
Part Number: TIDA-010083 Other Parts Discussed in Thread: TPS23758 Hello everyone,
Regard TIDA-010083 the standard is IEEE802.3at from my search AT just for high power ,
are it's COMPATIBLE with IEEE802.3af ??
Thanks
Hi Joseph,
For unused magnetics connection, it is okay to leave floating or terminate to ground.
I see some possible issues with this PoE termination, please refer to the termination scheme shown in this reference design for PoE:
https://www.ti.com/tool…
Part Number: TIDA-010083 Hello,
I would like to use your design reference TIDA-010083 but I can't find an equivalent of the 750318525 transformer, do you know of an alternative active part on the market?
Thank you in advance, Sébastien Moya …
Part Number: TIDA-010083 Hi,
I'm trying to get my head around the isolation requirements for PoE, and was wondering if you could help out with some comments on the design choices in component selections and layout for the TIDA-010083 reference design…
Hi Frankie,
Thank you for providing the information so clearly. The Center taps bussed together never works, even without the POE circuitry.
We have a POE reference design board here: https://www.ti.com/tool/TIDA-010083
The schematics and BOM are available…
Part Number: TPS23758 Other Parts Discussed in Thread: TIDA-010083 , I want to use the tps23758 to transfer a PSE(48V) to 5V output,the board tida-010083 is used for reference circuit.The circuit is as shown below.
D20、R66、F10 is not conneted now.
The…
Part Number: TPS23758 Other Parts Discussed in Thread: TIDA-010083 , Dear *,
I have few questions regarding TPS23758 and TPS23758 EVM
1) VB pin , in DS is stated it should be bypassed with 0.1uF and a 6.2V zener diode to GND.
In the TPS23758EVM-080 and …
Part Number: DP83867IR Other Parts Discussed in Thread: TIDA-010083 Hi team,
My customer referred to TIDA-010083 to design a 1000M PHY. Could you help check below schematics?
Below are what I've found,
1. When powering VDDA1P8 with an external supply…