Part Number: TIDA-01187 Other Parts Discussed in Thread: OPA695 Hi Team,
Our customer is looking for a high speed LED light modulator. He wants to send a binary signal (LED ON / OFF) using LED or laser with MHz frequency. Is the TIDA-01187 reference design…
Part Number: TIDA-01187 Hi,
I run into problems to open the file TIDA-01187_A.brd which is zipped in tidrpy8.zip.
Eagle is not able to import it. Could you tell me or send me an updated version?
Thanks,
Michael
link: www.ti.com/.../tidrpy8
Part Number: TIDA-01187 In the document: LIDAR-Pulsed Time-of-Flight Reference Design Using High-Speed Data Converters you describe the hardware implementation for ToF or DSP based options. What is the advantage of the second one? Would you point me to…
Part Number: TIDA-01187 Other Parts Discussed in Thread: LMG1020 , DAC5682Z , TIDA-01573 , OPA695 Hi.
We are trying to combine TIDA-01187 with 01573 for high-speed & narrow pulse width LIDAR.
The whole frame structure is surely TIDA-01187, but some parts…
Part Number: TDC7201 Other Parts Discussed in Thread: TIDA-01187 , , THS4541 Hi,
Now my customer is designing with reference to TIDA-01187. Specifically, it includes PD detection circuit and LD drive circuit. They are considering to replace the conversion…
Part Number: TIDA-01187 Hello
We see the feature of the reference design TIDA-01187 is suggested measurement range from 1.5m to 9m, and we'd like to know if possible to use the reference design to modify for longer distance range measurement, like increase…
Hello Burak,
1) Are you saying you want to bypass the TIA? You would need a way to convert the current input source to a voltage which is best done by an amplifier configured in a transimpedance manner. Not sure about the detection speed for the MCU…
Part Number: TDC7201 Other Parts Discussed in Thread: TIDA-01187 Dear team,
Customer want to know if we have some IRLED brand to recommend to work with TDC7201?
Thanks.
Best regards,
Sammi
Hello Kai,
The analog input bandwidth (-3 dB) is 540 MHz. 5 nS = 200 MHz, so, depending on your requirements, this might be good enough. Additionally, you can see our LIDAR reference design that uses the ADC3244 at the below link.
http://www.ti.com/tool…