Part Number: TM4C123GH6NMR Hi team,
May I know is there any spec different for the TM4C123GH6 NMR and the TM4C123BH6 ZRB ?
The NMR part datasheet on TI.com as below link is showed ZRB rather than NMR.
And it looks naming rule not seeing NMR on the datasheet…
Part Number: TM4C123BH6ZRB Hi team,
Just like the title says, when will the new, redesigned laminate device be available for ordering?
Right now I just see the TM4C123BH6ZRB and similar devices still in last time buy.
Thanks,
Jacob
Part Number: TM4C123BH6ZRB Hi team,
I had just released a program using the TM4C123BH6ZRBI7R from when it was ACTIVE status. Now I see it has been moved to Last Time Buy. What caused the sudden change?
What TM4C device should I move to which will cause…
Part Number: TM4C123BH6ZRB Hi,
in ADC register ADCCTL I found a Bit called "ADC_CTL_DITHER"; I am not sure of setting it.
-> Manual desciption: 'When taking multiple consecutive samples with the ADC Module, the DITHER bit should be enabled.…
Part Number: TM4C123BH6ZRB Hi,
I've ported our bootloader to the TI hardware. The last step is to set the stack pointer before jumping into the application what usually can be done through some inline assembly like
void __set_MSP(uint32_t val) { …
Part Number: TM4C123BH6ZRB Hello
I have a minimal program which fits in the first kB. The hex-tools output produces the intel hex file. It shall be loaded with Uniflash.
However, the .hex file is somehow not written, the memory region from 0x00 to 0x400…
Part Number: TM4C123BH6ZRB Team,
Our customer wants to know if they should move ahead with doing their layout for the ZRB package (157 ball BGA) with a 4 layer, top side only design. This means placing all the decoupling caps on the top side.
I looked…
Part Number: TM4C123BH6ZRB Hey,
we use TM4C123BH6ZRB bootloader to flash the TIVA via SPI.
On SPI master (i.MX 6) which downloads the binary file I have to set the block transfer size (must be a multiple of four).
Now I'm wondering about different max…
Part Number: TM4C123BH6ZRB Part: TM4C123BH6ZRB
Am using latest version of uniflash on Fedora Linux.
I can erase the Tiva via commandline:
/usr/local/uniflash_6.4.0/dslite.sh -e -c /tftpboot/sm400/Tiva_TM4C123BH6ZRB.ccxml -a Erase # ***** WORKS ****…
Hello Ralph,
meanwhile I solved it!
-> Hardware watchdog caused the problem!
Assumption: By expanding Flash area more time for initializing is neccessary.
Now HW WDG is not so short (I contract it when initialization is done) so that this Problem doesen…