Part Number: TMDX654IDKEVM Other Parts Discussed in Thread: PROFIBUS Hi guys,
I have the TMDX654IDKEVM board and after startup it is running in to a kernel panic error.
And I am getting also an unhandled exception EL2 when it is not a panic error.
So,…
Hi Zdenek
The dev team was able to reproduce the issue on SDK8.0 , but as mentioned are not able to reproduce the issue on latest SDKs.
How important is this for you to root cause and and understand vs running with the latest SDK.
For us to do all the…
Part Number: TMDX654IDKEVM We have purchased the TMDX654IDKEVM eval board www.ti.com/.../TMDX654IDKEVM in order to test the ProfiNET interface on our devices. But right from the beginning the board doesn't boot. Here is my error description. I hope you…
Hello Pekka,
Pekka Varis said: Can you give an example of how to you want it done so it would not be covered up? Do you mean test needs to be done using 2 boards, not the single board and 2 Ethernet devices above?
The start time of the PPS currently depends…
Part Number: TMDX654IDKEVM
ICSSG driver drops some RX frames, because flags in XDP structure are uninitialized.
Credit goes also to people from CouthIT who debugged it to the flag.
Following patch fixes that:
fix.xdp.struct.init.diff.txt
…
Part Number: TMDX654IDKEVM TI Linux CI/CD has instructions how to build images here:
https://software-dl.ti.com/cicd-report/linux/index.html?section=snapshot&platform=am65xx&snapshot=cicd.kirkstone.202402291453
To rebuild all of the images that…
Hello Lukas
Yes since the implementation has been rejected in upstream Linux, the patch will not be carried forward to the next release.
Marking this closed
Part Number: TMDX654IDKEVM Hello,
the PRU ICSSG interfaces bounce between link states with PHYs in interrupt mode
The issue is reproducible by controlling interface state. In a few repeating calls "if l set eth3 down", "if l set eth3 up" occurs link state…