Hi Jacky,
Most of the listed features can be supported by DaVinci DM3725/30 based system but it is needed SW implementation. Hire are some links to useful software libraries and applications:
processors.wiki.ti.com/.../Software_libraries
www.ti.com/…
Hi Srikanta,
Go through these links to understand xDAIS/xdm and porting a code on DSP and making it xDAIS compliant
processors.wiki.ti.com/.../Porting_GPP_code_to_DSP_and_Codec_Engine
www.ti.com/.../tmdxdaisxdm
XDM interface is mainly for audio/image…
The alg.h and _alg.h files are available with the XDAIS Developement Kit vesion4.1 @ http://www.ti.com/tool/tmdxdaisxdm
Checked the earlier 7.x versions, 6.x and 5.x versions. None have the two files in question.
Search for xDAIS Developer’s Kit v4.0 …
Other Parts Discussed in Thread: TMDXDAISXDM Hi there, I'm embarking upon a project in which I'd like to stream either VP8 or H. 264 from an OMAP 4-based device. I have a couple questions about it:
- Is VP8/H 264 encoding AND decoding hardware…
This doesnt mean that only TI supplied codec can be used in this context of discussion. You can add wrappers to your codec as per this standard and use.
XDM compliance means the codecs should follow some standards defiintions, interfaces as defined by…
Other Parts Discussed in Thread: TMDXDAISXDM , OMAP-L137 Hi,
I am a beginner to XDAIS and need some help in running an XDAIS example projects on C672x platform.
For XDAIS Developer's Kit, I downloaded v5.21 from location mentioned on "http://focus.ti.com…