XING,
XING CUI said: What is the maximum frequency of TXFULL and RXEMPTY in the DSP SPI register? What could be the reason for its slowing down?
-----> your question is not understandable...
-------> What do you mean by the max frequency of TXFULL…
compiler version is OK.
What is your CCS version?
---
More over your query is not understandable.
Expand your question with more screenshots and things that your are trying to do....
Regards
Shankari G
Part Number: TMS320C6678 Hi Ti
We have a product use TMS320C6678 DSP, and we have a question, how about the life time of TMS320C6678. Thanks.
regards
wenbang
Part Number: TMS320C6678 I have rebuild the ndk 2.21.02.43 for C6678,but get the library without the same size of the ndk installed.how to rebuild the ndk to get the same library files like ti released?
Part Number: TMS320C6678
Hi TI Team,
We want suggestions on the matrix keypad interface with the GPIO interrupt-based at the TMS320C6678. Because there is low power(1.8V).
If there is any need for additional hardware or IC during the implementation, Please…
Part Number: TMS320C6678 Hi,
We want to reduce the speed of the core(s) that's why we want to change the frequency on the core(s) individually or in groups(TMDSEVM6678LE). We want to know about the possibility of the frequency set being changed between…
Part Number: TMS320C6678
Hi,
We generated individual interrupts at each GPIO pin. But, We facing the multiple interrupt generation at GPIO pins into a signal. We want to use multiple interrupt generation using the Event Combiner for the GPIOs( into…
Hi,
As per the snippet of code, we got the frequency but have some doubts about it.
1. Can we implement it into the all-core or individual core?
2. We used the code (as per the code's snippet) here is the image,
3. After the (2), Can we use this…
Part Number: TMS320C6678 Thanks for the support in advance.
I just started studying edma3, and I copied the main.c (in pdk_c667x_2_0_16\packages\ti\csl\example\edma\edma_test) into my previous project, and the build was not successful.
the Problems window…