Part Number: TMS320F28052 Tool/software: Immediately after debugging “C28xx: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x3f2711: (Error -1066 @ 0x3F2711) Unable to set/clear requested breakpoint. Verify that the breakpoint address…
Part Number: TMS320F28052 Hi, I have an issue with my debbuger, an XDS110 debug probe connecting to the F28052 micro-controller.
I am able to connect to the micro and flash the program into it, but whenever I enable the micro to begin running an applicaton…
Part Number: TMS320F28052 Hi,
1) Is it okay if the yellow pins are open when JTAG is not connected?
2) Is the following how to handle unused pins?
GPIO ・ ・ ・ Open and set to "output"
3) Are there any requirements other than the following regarding…
Part Number: TMS320F28052M Other Parts Discussed in Thread: DESIGNDRIVE Hi,
What is the suggested upgrade path for our drive design to support an absolute position feedback sensor, such as HIPERFACE, SIN/COS, HIPERFACE DSL, etc?
We current use the TMS320F28052M…
Part Number: TMS320F28386D Other Parts Discussed in Thread: C2000WARE Hi C2000 Champ !
As I checked the availability via C2000-IEC60730-SW-PACKAGE page. I am not able to find TMS320F28386x device in the list.
Can you please clarify if TMS320F28386x would…
Other Parts Discussed in Thread: TMS320F28052 Re: TMS320F28052 Analog Port Injection Current
I need to know how much analog input injection current, over the uP's temperature range, will start to affect adjacent/other A/D inputs.
This isn't a normal operating…
TMS320F280049C will not support InstaSPIN Motion. The only device we support InstaSPIN Motion will be TMS320F28068/9M and TMS320F28052/4M. For more details, please refer to https://www.ti.com/microcontrollers/c2000-real-time-control-mcus/applications/instaspin…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Sean,
Please try the attached updated Flash Plugin file. After downloading, rename the extension as "dll" and place the Flash28xx.dll file at C:\ti\ccsv6\ccs_base\DebugServer\bin. Make sure to close the CCS when replacing this file and reopen…
A: The following C2000 device families include the F05 flash technology.
Delfino devices in the TMS320F28335 and TMS320F28235 family
Piccolo devices in the TMS320F2806x, TMS320F2805x, TMS320F2803x and TMS320F2802x families.
Fixed-Point devices in the…