Part Number: TPD1E10B06-Q1 Dear all
Could you tel me the products that are most suitable for LIN?
Specification Automotive Grade Use only LIN 1ch
Masa0301
Part Number: TPD1E10B06-Q1 Other Parts Discussed in Thread: TPD1E10B06 , STRIKE
When I read TPD1E10B06 datasheet, I can't understand what is the DC breakdown voltage. And what is the difference between DC breakdown voltage and clamping voltage? when will…
Part Number: TPD1E10B06 Other Parts Discussed in Thread: TPS25947 , TPS25947EVM , TVS1801 , TVS1800 , TVS2200 Hi, TI expert
The customer company has a question about selecting a TVS device with a surge function.
Q1) Can I confirm what level the TPD1E10B06…
Other Parts Discussed in Thread: TPD4E05U06-Q1 , TPD1E01B04-Q1 , TPD1E05U06-Q1 , TPD1E10B06-Q1 , TPD1E05U06 , TPS25740B Hello,
I am searching the ESD Protection Device for Type-C' s CCx, DM and DP pins.
I wonder what is the nominal working voltage of these…
Part Number: TPD1E01B04-Q1 Other Parts Discussed in Thread: STRIKE , TPD1E10B06-Q1 , TPD2E2U06-Q1 , TPD1E01B04 , ESDS312 , TPD1E1B04 , ESD321 Dear team,
My customer plans to use this device, and their test requirement is as below. Their requirement is 25kV air…
Hi Matt,
Thanks for the detailed answer. Below are the follow-up questions:
1. As you mentioned, TPD1E10B06-Q1 is 6A rated and can sustain surges up to 252V peak with 42-ohm resistor. So, is it right to note that TPD1E10B06-Q1 cannot pass IEC 61000-4-5…
Part Number: TPD4E02B04-Q1 Other Parts Discussed in Thread: TVS0500 , TPD1E10B06 , TPD1E05U06 , TPD4E02B04 , ESD122
Hi Erika,
I hope you are doing good.
I want to put my design to esd protection. That's why, I realized TPD4E02B04-Q1 ESD Protection Diode…
Other Parts Discussed in Thread: TPD1E10B06 , TPD1E05U06-Q1 I am designing a USB to PS2 circuit and have to provide +5V for a keyboard and mouse output. I need to provide protection for these output supplies. It has been suggested that I use an inductor…
Part Number: TPD1E10B09-Q1 Other Parts Discussed in Thread: TPD1E10B06 Hi there,
I would like to use the TPD1E10B09-Q1 product for my hall sensor ESD protection application. Is it OK for hall sensor signal levels ? If not do you have any other suggestion…
Part Number: TPD1E01B04-Q1 Other Parts Discussed in Thread: ESD401 , TPD1E10B06 ,
Hi Erika,
Could you help to recommend the ESD diode for the UB933 and UB954? What’s the maximum IO cap for the FPD-link for these two parts?
Customer want to know what…