Part Number: TPS22904 Hello, guys.
It is about the TPS22904 load switch. I downloaded CAD/CAE symbol from your site and there is a mismatch between schematic CAD symbol and datasheet info.
Datasheet says that pin A1 is Vin and pin A2 is Vout. On the other…
Part Number: TPS22904 Other Parts Discussed in Thread: TPS22901 , TPS22902 Is the pinout indicated in the datasheets for the two subject parts (TPS22904 and TPS22902B) correct (i.e. mirrored)? If so, I am looking for a 22904 pin-compatible part with a…
Part Number: TPS22904 Other Parts Discussed in Thread: TPS22915 , TPS22916 Hi,
i have a dual supply voltage system with VDD/VSS= +2.5V/-1.0V, and the supply current is 150mA.
LDO is the power source of VDD(+2.5V); DC/DC convertor is the power source of…
Hello Victor,
Please take a look at the following devices:
TPS27081A
TPS22904
TPS22921
They're in order starting from lowest Iq downt to highest Iq (of these specific options). I excluded choices with inventory < 10000. They all support 1.8V - 3.3V.…
Other Parts Discussed in Thread: TPS22904 , DLPC150 , SN74ALVC08 , CC2564 , ADS1255 , TMP006 , HDC1000 Hi,
I have a Tiva C project working on 2.10.1.38 TI RTOS version. I just migrated it to TI RTOS 2.16.1.14; following the migration guides. Pasted below is…