Hi Benny,
Thank you for your answer.
So if I understand:
- with the TPS2513 in 5W mode the maximum negociated current to consume is 1.5A (divider 1 BC1.2)
- with the TPS2513 in 10W mode the maximum negociated current to consume is 2A (divider 2)
-with…
Part Number: TPS2513 Hi team,
This part supports USB charging specification, BC1.2. Is there the emulator to evaluate the BC1.2 charging operation of this part?
Regards, H.Someno
Part Number: TPS2513 I would like to know the specific contents of DCP Auto-Detect.
How does the TPS2513 identify a compliant charging standard when a charging device is connected?
What does TPS2513 recognize and switch the following modes?
Part Number: TPS2513 Other Parts Discussed in Thread: TPS564201 Hello,
I've been working with TPS2513 for new chargers and it does charge but only at 1A each port, checking DP and DM data lines are at 0.7~1.2V each(depending the smartphones tested).…
Part Number: TPS2513 Other Parts Discussed in Thread: TPS2561 Hi,
I have an urgent request from my customer:
would it be possible to use TPS2513 is that schematic (see attached). They would want to place a Power Switch in front of the device so on the…
This behavior seems to be driven by the connected device rather than the TPS2513. There is nothing the the TPS2513 design that would drive just one to the two data lines to 1.2V.
Regards,
Chuck
Part Number: TPS2513 Hi everyone, I have a problem with TPS2513, in the project I design, I use a 10W aplication. I looked at all the datasheet, and I did everything by the instructions. When I test PCBs and connect different phones, the highest current…
Part Number: TPS2513 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models I am attempting to compile the .lib pspice file for the TPS2513DBVR using Tina 9.3.150.328 and I'm getting a message stating, "Invalid device: $CDNENCSTART…
Part Number: TPS2513 Other Parts Discussed in Thread: TPS25810 Hello dear USB Team,
I want to use the TPC2315 to charge a device via an USB Type-C connector. WIll there be any problems, if the USB2.0 pins within the Type C connector will be supplied…
Part Number: TPS2513 Other Parts Discussed in Thread: TPS2546 Hi,
I am planning a USB-charger where we use the TPS2513 to negotiate the charging current.
The only problem is the comparably high supply current of the TPS2513 at around 150uA.
I would rather…