niwao said: ① Is the short mode switching condition just to connect D+/D- with 0 to 200Ω (max)?
This is correct and required for DCP detection by the sink device. I would recommend taking a look at the TPS2514A datasheet which has explanation about when…
Part Number: TPS25810EVM-745 Hi,
Can you please share Altium design file for TPS25810EVM-745?
I would like to reuse it for one of the projects. Thank you.
Regards,
Sanjay R. Pithadia
Hi Chase,
1) Unfortunately I do not see in the white paper where is says 3V. As Eric described, USBC (even 2.0, 3.1, and BC1.2) are all 5V.
2) If the TPS25810 is in the end equipment, the IC's min recommended input is 4.5V so yes there needs to be a…
Other Parts Discussed in Thread: TPS25810 , TPS25810EVM-745 Hi all Would you minf if we ask TPS25810? Do CC1 and CC2 have reverse protection? We can't find it on the datasheet. Kind regards, Hirotaka Matsumoto
TPS25810